Renaming a User or Role - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0

Security Administrator System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-1201528
Version
12.0
Revision date
2022-08-05

About this task

Note: The Metasys Security Administration tool cannot rename the Active Directory service users because their names are controlled by Active Directory services. If you rename an Active Directory service user, a Metasys System Administrator must synchronize the user before the user can log in to the Metasys system. See Synchronizing an Active Directory Service – User Account.

Procedure

  1. Select the user or role to rename.
  2. On the Edit menu, click Properties. The User/Role Properties tab of the User/Role Properties dialog box appears.
  3. Type a new name in the User Name field.
  4. Click OK.