Placing Time-of-Day Restrictions - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0

Security Administrator System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-1201528
Version
12.0
Revision date
2022-08-05

Procedure

  1. Select the user to configure.
  2. On the Edit menu, click Properties. The User Properties dialog box appears. See Figure 1.
  3. Select the Time Sheet tab. See Figure 1.
  4. Select the times when users can access the system by clicking time slots to toggle between Access Allowed (blue highlight with white text) and Access Denied (no highlight with black text). See Table 1.
  5. Click OK.