Creating a Metasys local user account - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0

Security Administrator System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-1201528
Version
12.0
Revision date
2022-08-05

Procedure

  1. Log in to the Metasys server or SCT with a Metasys Administrator account.
  2. On the Main screen, click Tools > Administrator. The Security Administration window appears (Figure 2).
  3. On the Insert menu, click New User. The User Properties tab of the User Properties dialog box appears. See Figure 1.
  4. Fill in the information and click OK. The New User appears in the Roles and Users tab.
  5. Set the other properties and define System Access Permissions for each Metasys local User. For details, see the Detailed Procedures sections that follow, then see System Access Privileges.
  6. Close the Security Administration window.