Removing User Access to Active Directory Service from the Metasys System - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0

Security Administrator System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-1201528
Version
12.0
Revision date
2022-08-05

Procedure

  1. Log in to the Metasys server or SCT with a Metasys Administrator account. On the Main screen, select Tools > Administrator. The Security Administration window appears.
  2. Select the Active Directory service user you want to remove as a Metasys system user. On the Security Administration window, click Edit>Delete.
  3. Click Yes to confirm the user deletion. This Active Directory service user is removed as a Metasys system user and the Active Directory User list is refreshed.