Assigning Access by Using the User Properties or Role Properties Dialog Boxes - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0

Security Administrator System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-1201528
Version
12.0
Revision date
2022-08-05

Procedure

  1. Select the user or role.
  2. On the Edit menu, click Properties. The User Properties tab of the User Properties dialog box appears (see Figure 1) or the Role Properties tab of the Role Properties dialog box appears (Figure 1).
  3. Select the Navigation tab (Figure 1 for user or Figure 1 for role).
  4. In the Available Views list, click one or more user views to assign.
  5. Click Add.
    Note: To remove user Navigation View Permissions from the user or role, click one or more user views in the Assigned Views list and then click Remove.
  6. Click OK.