Assigning System Access Permissions - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0

Security Administrator System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-1201528
Version
12.0
Revision date
2022-08-05

Procedure

  1. Select the user or role.
  2. On the Edit menu, click System Access Permissions. The System Privileges dialog box appears.
  3. Select an available privilege using Table 1.
  4. Click Add.
  5. Click OK.

    The System Access Permissions are assigned to the selected user or role.

    When you are viewing user system privileges, select the Summarized tab to view all system privileges assigned to the user either directly or by a role. You cannot add or remove privileges from this tab, and it does not appear when viewing role system privileges.