Status Messages appear in the DB Connection Parameters Status section.
| Message | Description |
|---|---|
| Ready | The tool is ready for action. |
| Metasys III Device Manager | The device manager is running. You can not update the connection configuration until you stop device manager and relaunch the application. |
| Error opening/reading configuration file | The connection configuration is locked by another process or missing and can not open for reading. |
| Error writing to the configuration file | The connection configuration is locked by another user or missing and can not open for writing. |