Passwords - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0

Security Administrator System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-1201528
Version
12.0
Revision date
2022-08-05

Passwords are the SQL Server Login account passwords defined in the server instance that is specified in the Server name field. The password length is not limited by DBCCT; however, the maximum password length in SQL Server is 128 characters. DBCCT does not require or prevent the user from entering complex passwords. The complex passwords policy is enforced by SQL Server. This tool only sets the passwords to match the passwords set in SQL Server for the accounts and connection strings described in Table 1.