Metasys software installs Windows services. These services include:
- Device Manager (MetasysIII Device Manager)
- ADS/ADX Action Queue (MetasysIII Action Queue)
- Advanced Reporting Cache Refresh (Metasys Report Cache Refresh)
Upon startup, DBCCT checks the status of the Metasys services as shown in Table 1.
The tool displays only the tabs and edit fields needed to configure the installed
services. You cannot access these fields and tabs until all installed services are
stopped. If the tool detects any services running, the editing fields appear as
read-only and a message indicates the detected service. We recommend stopping these
services before using the DBCCT.
| Application Name | Service or Application Pool Name |
|---|---|
|
ADS\ADX\OAS |
UI_AppPool ActivityService_AppPool Metasys.ActivityService EventService_AppPool Metasys.EventService TimeSeries_AppPool Metasys.TimeSeriesService SchedulerService_AppPool Metasys.SchedulerService AuthenticationService_AppPool HealthService_AppPool ObjectService_AppPool UserService_AppPool Metasys III Device Manager Service Metasys III Action Queue Service Metasys app pool |
|
Advanced Reporting System (ARS) |
Metasys Report Cache Refresh |
|
Metasys UI (Release 8.0 and 8.1) |
UI_AppPools |