User Properties Tab – Active Directory Service User - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0.50

Security Administrator System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-1201528
Version
12.0.50
Revision date
2023-06-02

The User Properties tab for an Active Directory service user defines general information about the user. The Active Directory service domain server sets and controls the fields that appear as read-only (Figure 1). The Metasys system controls all other fields, which are user modifiable and do not affect the account since it is maintained by the Active Directory service domain server.

Figure 1. User Properties Tab – Active Directory Service User

Table 1. User Properties Tab Parameters – Active Directory Service User

Field

Description

Default Value

Required

Active Directory User Name

Displays the login name of the Active Directory service user. This is a read-only field.

Yes

Active Directory Description

Displays a description of the Active Directory service user. This is a read-only field.

No

Password

Displays a dimmed field because the password is defined and maintained with Active Directory services.

Verify Password

Displays a dimmed field because the password is defined and maintained with Active Directory services.

View Blocked Words List

Displays a dimmed View Blocked Words List link.

View Password Policy

Displays a dimmed link to the rules for password complexity.

Minimum Password Length

Displays a dimmed field because the password is defined and maintained with Active Directory services.

Maximum Password Length

Displays a dimmed field because the password is defined and maintained with Active Directory services.

Single Access Active Directory User

Allows the Active Directory service user to log in to the account once. After logging in once, the account becomes disabled.

Cleared

No

Temporary Active Directory User

Allows the Active Directory service user to access the system as a temporary user. The user can access the account as long as it has not expired. When expired, the user is logged out of the system.

No

Expires On

Allows the administrator to specify the date on which a temporary user's account expires. The account expires at the end of the specified date (midnight), after which the user can no longer access the system.

The default value is the current date.

Yes, if temporary user selected.

Metasys Access Suspended

Allows the administrator to suspend an Active Directory service user account from accessing the Metasys system. This option becomes selected automatically if the Active Directory service user is disabled or deleted from Active Directory services.

Note: If the Active Directory service user's account is enabled again or re-added, you must manually clear the Metasys Access Suspended check box.

Cleared

No

Active Directory Account Deleted

Displays a dimmed field because this property is controlled by Active Directory service. If this option is selected, the Active Directory service user account cannot be found and may have been deleted.

Cleared

No

Active Directory Account Disabled

Displays a dimmed field because this property is controlled by Active Directory services. If this option is selected, the Active Directory service user account has been disabled within Active Directory services.

Cleared

No

User Can View the Item Navigation Tree (Default Tree)

Designates that a user can view the All Items navigation tree.

Selected

No

User Can Disable Alarm Pop-ups

Allows the user to disable or enable alarm windows.

Selected

No

Access Type

Specifies the type of access the user has to the system.

Standard

Yes