User Profile Tab - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0.50

Security Administrator System Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-1201528
Version
12.0.50
Revision date
2023-06-02
Language
English

The User Profile tab includes more details about the user. The administrator sets the language and the default navigation view that the user sees when logging in to the system (Figure 1). For the User Profile of an Active Directory service user, the first three properties appear dimmed because they are read from and maintained by Active Directory services.

Note: Other languages are available only when the associated language files are installed on the server or supervisory device. Multiple languages can be installed on the Metasys server and SCT. Only a single language can be installed on the NAE/NCE, including the NAE85.
Figure 1. User Profile Tab - Metasys Local User

Table 1. User Profile Tab Parameters

Field

Description

Default Value

Required

Full Name 1

Displays the full name of the user.

No

Email1

Displays the email address of the user.

No

Phone Number1

Displays the telephone number of the user.

No

Language

Displays a drop-down list of the site supported languages.

Note: Each time you change the language, you are required to change your password the next time you log in so that the new password you define is verified against the requirements of the new language.

English (United States)

Yes

Default Navigation View

Displays a drop-down list of available navigation views. The selected view is the initial view used upon logging on to the account.

All Items Navigation Tree

Yes

Enable Audible Alarm

Allows user to hear a sound when an alarm occurs.

Selected

No

1 For an Active Directory service user, this field is read-only and the following text is appended to its property name: (from Active Directory).