Backing up and restoring the Security Database with SCT backs up and restores the Active Directory service users, Metasys local users, and roles for a Metasys server.
The following Metasys Active Directory service configuration information is stored in the Security Database and backed up or restored along with other Security data:
- Active Directory Service Authentication Enabled or Disabled
- Windows Workstation SSO Enabled or Disabled
- Login Page Default Domain Selection
- Active Directory Service Service Accounts
Settings from the backup replace existing settings on the targeted device during a restore operation.