Role Properties Tab - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0.50

Security Administrator System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-1201528
Version
12.0.50
Revision date
2023-06-02

The Role Properties tab defines the general information about the Role Users tab (Figure 1).

Figure 1. Role Properties Tab

Table 1. Role Properties Tab Parameters

Field

Description

Default Value

Required

Role Name

Displays a unique name for the role.

Role Name

Yes

Description

Displays a description for the role.

---

No