Navigation Tab - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0.50

Security Administrator System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-1201528
Version
12.0.50
Revision date
2023-06-02

The Navigation tab allows administrators to specify which user navigation views a user can access (Figure 1). This tab is the same for both the Metasys local system user and the Active Directory service user, but is disabled in the SCT.

Figure 1. Navigation Tab - User

Table 1. Navigation Tab Parameters

Field

Description

Default Value

Available Views

Displays the user navigation views to which the selected user is not assigned.

All available views

Assigned Views

Displays the user navigation views to which the selected user is assigned.

Add

Moves the user navigation views from the Available Views list box to the Assigned Views list box.

Remove

Moves the user navigation views from the Assigned Views list box to the Available Views list box.