Setting Password Account Policies - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0.50

Security Administrator System Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-1201528
Version
12.0.50
Revision date
2023-06-02
Language
English

Procedure

  1. Select the user to configure.
  2. On the Edit menu, click Properties. The User Properties dialog box appears. See Figure 1.
  3. Select the Account Policy tab.
  4. Select options using Table 1 (Metasys local users) or Table 2 (Active Directory service users).
  5. Click OK.