Creating a new role in SMP or SCT - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0.50

Security Administrator System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-1201528
Version
12.0.50
Revision date
2023-06-02

Procedure

  1. On the Insert menu, click New Role. The Role Properties tab of the New Role dialog box appears (Figure 1).
  2. On the Role Properties tab, fill in the information. See Table 1.
  3. On the Users tab, assign users to the new role using the Add button. See Figure 1.
  4. On the Navigation tab, assign access to user navigation views using the Add button. See Figure 1.
  5. Click OK.
    The New Role appears in the Roles and Users tab.