Selecting a Default Domain for Active Directory Service – Users - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0.50
Security Administrator System Technical Bulletin
- Product
- Building Automation Systems > Building Automation Systems > Metasys System
- Document type
- Technical Bulletin
- Document number
- LIT-1201528
- Version
- 12.0.50
- Revision date
- 2023-06-02
Procedure
-
Log in to the Metasys server or SCT with a Metasys Administrator
account.
-
On the Main screen, click > . The Security Administration window appears (Figure 1).
-
On the Security Administration window, click > . The Configure Active Directory dialog box appears (Figure 2).
-
Using the Login Page Default Domain Selection option, select
the domain that the Metasys SMP UI presents as the default selection on the
Metasys login screen. This default applies to all users, regardless of a
particular user’s domain; therefore, if multiple domains are used, you may want
to select the domain that applies to the majority of users.
-
Click Save or Apply to save this
change. Clicking Save returns you to the Security
Administration screen.