Detailed Procedures - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0.50

Security Administrator System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-1201528
Version
12.0.50
Revision date
2023-06-02

Changes made to user accounts in the Security Administrator system no longer affect all Metasys system components that reside on the same computer. For example, on a computer that has both an ADS and SCT installed, changes you made in the Security Administrator system do NOT affect both the ADS and the SCT.

For more information on Security Databases at Release 7.0, refer to the SCT: System Configuration Tool Help (LIT-12011964) .

Note: Some of the procedures in the following sections apply only to networks that have the Microsoft Active Directory service technology implemented at the site. If you are enabling the Active Directory service for use by the Metasys system, see Configuring Active Directory Service for Metasys System Use.