Status Messages - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0.50

Security Administrator System Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-1201528
Version
12.0.50
Revision date
2023-06-02
Language
English

Status Messages appear in the DB Connection Parameters Status section.

Table 1. Status Messages
Message Description
Ready The tool is ready for action.
Metasys III Device Manager The device manager is running. You can not update the connection configuration until you stop device manager and relaunch the application.
Error opening/reading configuration file The connection configuration is locked by another process or missing and can not open for reading.
Error writing to the configuration file The connection configuration is locked by another user or missing and can not open for writing.