Server Name - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0.50

Security Administrator System Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-1201528
Version
12.0.50
Revision date
2023-06-02
Language
English
The ADS DB Server field contains the name of the SQL server that hosts the server databases. In a single box ADX, the name is the same as the application server. In a split ADX configuration, this field contains the database server name. This field format is the standard SQL connection string syntax. Metasys supports using SQL Server that has named instances.
Table 1. Server Names
Format Example Format with Instance Name Example with Instance Name

protocol name:server name]

(local) or localhost

protocol name:server name\instance

tcp:localhost\SpecialSqlServer

IP address, port number

159.222.10.194, 1500

IP address\instance name, port number

159.222.10.194\SpecialSqlInstance, 1500