About this task
Note: This procedure uses SQL Server
2017 Reporting Services but the steps are similar for other editions of SQL
Server Reporting Services.
Procedure
-
Start Report Server Configuration Manager. The Report Server Configuration Connection dialog box appears.
Note: If the Report Server Configuration Connection dialog box does not appear, you do not have installed SQL Server Reporting Services. For more information see Installing SQL Server Reporting Services for SQL Server 2017
-
In the Report Server Instance field, select the correct instance name. Click Connect.
Figure 1. Instance Selection
-
In the Report Server Status pane, verify Started is in the Report Service Status entry. If not, click Start.
Figure 2. Report Server Status
-
In the left pane, click Web Service URL.
- In the Report Server Web Service Virtual
Directory area, verify that a virtual directory appears
in the Virtual Directory field.
If any warning icons appear, address the issues. If you used a named
instance other than SSRS, the instance name is in either of these
formats:
Reports$instancename
orReports_instancename
. - In the Report Server Web Service URLs area, click the URLs hyperlink.
- In the Report Server Web Service Virtual
Directory area, verify that a virtual directory appears
in the Virtual Directory field.
If any warning icons appear, address the issues. If you used a named
instance other than SSRS, the instance name is in either of these
formats:
-
Windows web browser launches the Report Server Web service web page. The version shown depends
on which edition of SQL Server you installed. If you see Microsoft SQL Server Reporting Services Version
14.x.xxx.xxx on the web page, the web service URL configuration
is successful.
Note:
- This window may take up to 30 seconds to appear.
- If a prompt for a user name and password appears, type the administrator credentials, and click OK, or exit the web browser and relaunch the browser as an administrator. You can also avoid the prompt if you log in to the computer using the administrator user account.
- If the Report Server Web service window does not appear, or appears with an error, this indicates the configuration for the report server is incorrect. For more information, refer to the SQL Server Reporting Services troubleshooting section in SQL Server Installation and Upgrade Guide (LIT-12012240).
- In the left pane, click Database.
- In the right pane, in the Current Report Server Database area, verify that values appear in the Report Server Database area and no warning icon appears is visible.
-
In the left pane, click Web Portal
URL. Verify a virtual directory name is visible and no warning
icon appears. Windows web browser launches the SQL
Server Reporting Services web portal.
- To launch the web portal URL, click the URL link.
- If you see the SQL Server Reporting Services home page, the configuration is correct.
Note:- This window may take up to 30 seconds to appear.
- If a prompt for a user name and password appears, type the administrator credentials, and click OK, or exit the web browser and relaunch the browser as an administrator. You can also avoid the prompt if you log in to the computer using the administrator user account.
- If the Report Server Web service window does not appear, or appears with an error, this indicates the configuration for the report server is incorrect. For more information, refer to the SQL Server Reporting Services troubleshooting section in SQL Server Installation and Upgrade Guide (LIT-12012240).
Report services are configured and running correctly. To configure SQL Server Reporting Services for Metasys Advanced Reporting System, see Specific system requirements for the Metasys Advanced Reporting System.