Creating a new SQL Server user - Metasys - LIT-12012240 - Server - SQL Server - 13.0.50
SQL Server Installation and Upgrade Guide
- Product
- Building Automation Systems > Databases and Data Servers > SQL Server
- Document type
- Installation Guide
- Document number
- LIT-12012240
- Version
- 13.0.50
- Revision date
- 2024-04-09
- Product status
- Active
Procedure
-
Start SQL Server Management Studio for your version of SQL Server
software.
-
Enter the following:
-
Server
type: Database Engine
-
Server
name: This is the name of the database server (not the
web/application server). If you are using a SQL Server instance other
than MSSQLSERVER, include the SQL Server instance name in this format:
computername\instancename.
-
Authentication: SQL Server Authentication
-
Login:
existing SQL Server sa login (or another valid SQL Server login)
-
Password: existing SQL Server password for
sa user (or another valid SQL Server password)
-
Click Connect.
-
Press F7 if the Object Explorer Details window in the
right pane does not appear.
-
In the tree in the left pane, under the database server, expand the
Security folder and Logins
folders.
-
Right-click the Logins folder and select New
Login.
-
Select the SQL Server authentication method. Configure the
parameters for the new SQL Server user according to your company policies and
preferences. We offer the following recommendations:
- Specify
SSRSServiceAccount as the new
user name.
- Use a complex
password for the SSRSServiceAccount user.
- Make sure the
Enforce password expiration
is cleared.
- Keep the
Enforce password policy
selection selected.
-
Click OK. The new user is created.
-
Close all windows.
-
Go to Configuring SQL Server Reporting Services.