Appendix: Reporting services language support for Metasys Advanced Reporting System - Metasys - LIT-12012240 - Server - SQL Server - 13.0.50

SQL Server Installation and Upgrade Guide

Product
Building Automation Systems > Databases and Data Servers > SQL Server
Document number
LIT-12012240
Version
13.0.50
Revision date
2024-04-09
Product status
Active

The Metasys Advanced Reporting System displays reporting information in languages other than United States English when you install the correct language support for the ADX computer and you define a language in your Security Administrator System profile. This functionality is the same as using a non-English language on the ADX without the reporting system.

In addition to the language file installation and profile change for a non-English ADX, you also must download several supporting components to translate the main Toolbar, Report Toolbar, and Report is being generated message that appears in the Report screen. The supporting components are available for the following languages:

  • Czech
  • German
  • Spanish
  • French
  • Hungarian
  • Italian
  • Japanese
  • Korean
  • Norwegian
  • Dutch
  • Polish
  • Portuguese
  • Turkish
  • Chinese (Simplified)
  • Chinese (Traditional)

If you are installing a split ADX, perform the steps in this section on the web/application server only.

You can perform these steps before or after you install the ADX software with the Metasys Advanced Reporting System. If you do not follow this procedure, some of the menus and options do not appear in the desired language.