Determining the SNE IP address by using the SCT Pro - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

About this task

You can use SCT Pro to discover the SNE. To use the SCT Pro to discover the device and determine the IP address of an SNE, complete the following steps:

Procedure

  1. Open the SCT Pro dashboard.
  2. From the Utilities pane, click Discover. The Device Discovery page opens.
  3. Check the status to ensure the system listens for device wake-up messages.
  4. Click Discover. The table displays devices on the subnet.
    For more information, refer to SCT Pro Help (LIT-12013035).