Determining the SNE IP address by using the SCT Pro - Metasys - LIT-12013352 - M4-SNE10500-0 - M4-SNE10501-0 - M4-SNE11000-0 - M4-SNE11001-0 - M4-SNE110L0-0 - M4-SNE110L1-0 - M4-SNE22000-0 - M4-SNE22001-0 - Supervisory Device - SNE10 Network Engine - SNE11 Network Engine - SNE22 Network Engine - SNE Supervisory Network Engine - 12.0

SNE Commissioning Guide

Brand
Metasys
Product name
SNE10 Network Engine
SNE11 Network Engine
SNE22 Network Engine
SNE Supervisory Network Engine
Document type
Commissioning Guide
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active
Language
English

About this task

You can use SCT Pro to discover the SNE. To use the SCT Pro to discover the device and determine the IP address of an SNE, complete the following steps:

Procedure

  1. Open the SCT Pro dashboard.
  2. From the Utilities pane, click Discover. The Device Discovery page opens.
  3. Check the status to ensure the system listens for device wake-up messages.
  4. Click Discover. The table displays devices on the subnet.
    For more information, refer to SCT Pro Help (LIT-12013035).