Summary tab - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

The Summary tab (Figure 1) in the Site Management Portal UI provides a quick view of the status of the objects and items currently in your site.

Select, drag, and drop an object from the Navigation panel in the Display panel, and click the Summary tab. When you first click the Summary tab, the SNE requests the status of the items in the Display panel (Figure 1). This request may take a few minutes.

For additional information and explanations of the attributes found in the Summary and Diagnostic tabs, refer to the Object Help in the SCT: System Configuration Tool Help (LIT-12011964) or the Metasys Site Management Portal Help (LIT-1201793) .

Figure 1. SNE Summary Tab