Reset button - Metasys - LIT-12013352 - M4-SNE10500-0 - M4-SNE10501-0 - M4-SNE11000-0 - M4-SNE11001-0 - M4-SNE110L0-0 - M4-SNE110L1-0 - M4-SNE22000-0 - M4-SNE22001-0 - Supervisory Device - SNE10 Network Engine - SNE11 Network Engine - SNE22 Network Engine - SNE Supervisory Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document type
Commissioning Guide
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

The SNE features a recessed Reset button that is located directly above the Heartbeat LED. If you need to reset the SNE but retain the archive and stored historical data, issue a Reset Device command from the user interface. This type of reset is known as a soft reset.

To force an immediate restart of the SNE engine and a reset of the processor, press and immediately release the Reset button with an extended paper clip or mini screwdriver. This action is otherwise known as a hard reset or processor reset.

Important: During the reset, the SNE's archive database and any data the SNE has collected are lost.

The data includes all historical information, including alarm, trend, and audit trail data.

Note: Press the Reset button only if the network engine fails to respond and cannot be accessed by any user device. Do not press the Reset button unless you have tried other reasonable means to fix the problem.
Note: The network engine has a super capacitor that, when charged, keeps the unit powered up for 30 seconds.