Diagnostic tab - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document type
Commissioning Guide
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

The Diagnostic tab displays SNE hardware status information that may aid troubleshooting.

With the SNE object selected, click the Diagnostic tab to view current information about the SNE hardware status. Figure 1 shows an example.

Figure 1. SNE Diagnostic Tab

You can also select and drag Network Protocol objects into the Display panel and click the Diagnostic tab to view information for the selected Network protocol (Figure 2).

Figure 2. BACnet Protocol Diagnostic Tab