Warning banner - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

As an option, an SNE configured as a Site Director can have a Warning Banner enabled. The Warning Banner is a statement that always appears when operators log on the Site Management Portal of the engine. By default, the network engine is configured not to display a warning banner.

You have the choice of three different warning banners: U.S. Department of Defense (DoD), U.S. (General Services Administration (GSA)), or U.S. Department of Transportation (DOT) Federal Aviation Administration (FAA). The information in the text window is customized for the United Stated government agency where the Metasys system is installed. The reader must read and accept the conditions in the Warning Banner before logging on. The banner cannot be customized or its text be changed. For steps on how to enable or disable this banner, see Enabling and disabling Warning Banner.

Figure 1. United States DoD Warning Banner