Staged Firmware Version and Staged Files - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active
The SNE has two special attributes called Staged Firmware Version and Staged Files. These attributes support the dual partition format of the device's memory chip. As pictured below, these fields are usually empty. They are described as follows:
  • Staged Files: lists staged files that are set for activation at a later time. For example, if the code and archive database are set for later activation, this field would read Code, Archive Database. If this attribute is empty, no files are currently staged. Possible values: Code, Archive Database, Security Database, HTTPS Certificates.

  • Staged Firmware Version: indicates the engine firmware version that is staged for later activation. If this field is empty, no firmware files are currently staged. This attribute is in contrast to the Firmware Version attribute, which indicates the engine's firmware version that is currently active.

Figure 1. Staged Firmware Version and Staged Files attributes