SNE commissioning - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

SNE commissioning includes preparing the network engine for connectivity, connecting to the network engine, adding the network engine to the profile list in Launcher, and accessing and logging in to the engine's Site Management Portal UI.

Each Metasys network installation, commissioning, and configuration scenario is unique. In some scenarios, the network engines (on a Metasys network) may be commissioned and configured before they are installed and connected to the network; in other scenarios, the network engines are mounted and wired to the network before they are commissioned and configured.

Note: Network engine installation includes locating, mounting, wiring, and powering on an SNE. See Related documentation for references to SNE installation instructions for the various models.

The commissioning tasks, the task order, and the required attribute values (at commissioning) for a network engine are determined by the specific Metasys network installation, commissioning, and configuration scenario for the site. The commissioning procedures presented in this document are the procedures required for most scenarios regardless of when commissioning occurs.

The first task in commissioning an SNE is to establish a connection with the network engine through the Launcher. If the Launcher is not already installed on your machine, you are prompted to install it when you attempt to log in using the web browser. The Launcher is a software application installed on each client computer that lets you access any Metasys server or supervisory engine on the building network, regardless of its software version. For details, refer to the Launcher Tool Help (LIT-12011742) and the Launcher Installation Instructions (LIT-12011783) .

After a connection is established, you can then access the Site Management Portal on the SNE from the Launcher. See SNE connectivity for six typical network connection scenarios. See Site Management Portal user interface and Accessing Site Management Portal UI on an SNE for more information on accessing and navigating the Site Management Portal UI.

After you have accessed the Site Management Portal UI on an SNE, you can configure the engine:

  • object name and basic device parameters

  • host name (computer name), domain name, and network parameters

  • trusted certificates (optional)

  • time and date management parameters

  • alarm and event parameters

  • SNMP messages and the network management destination

  • network integrations

  • third-party protocol integrations

  • Site Director status

  • Advanced Security setting

After commissioning an SNE, you must configure the engine at the job site. The next section, SNE configuration, provides an overview of the sequence of steps needed to install, commission, and configure a new SNE.