Reset command device - Metasys - LIT-12013352 - M4-SNE10500-0 - M4-SNE10501-0 - M4-SNE11000-0 - M4-SNE11001-0 - M4-SNE110L0-0 - M4-SNE110L1-0 - M4-SNE22000-0 - M4-SNE22001-0 - Supervisory Device - SNE10 Network Engine - SNE11 Network Engine - SNE22 Network Engine - SNE Supervisory Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document type
Commissioning Guide
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

The Reset Device command in the Site Management Portal UI initiates an orderly reset that saves recent changes to the SNE archive database and restarts the engine's operating system. When the SNE requires a reset, the title bar of the object in the Display panel displays Reset Needed. A reset is required for new settings to take effect after making changes to the following attributes:

• APDU Retries

• APDU Segment Time-Out

• APDU Time-Out

• BACnet IP Port

• Computer Name

• Contact Person

• Domain Name

• Max APDU Length

• Network Address

• Port Number

• Read/Write Community

• SNMP DDA

• SNMP Management Device

• Serial Port 1 Cable Config

• Time Sync Period

Note: Changing the Computer Name value of the SNE forces a device reset.