Object name - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

The Name is an editable Object attribute on the SNE Focus tab that the Metasys software uses to identify the SNE in the Site Management Portal UI and in the SCT. The Object Name is a label only and may not be the same as the Computer Name. Changing the Object Name merely changes the name that you see in the navigation tree, alarm messages, trend reports, and other screens in the Site Management Portal UI and SCT that refer to the SNE. Changing the Object Name does not impact the object references or network communication with other devices on the site. You can change the Object Name at any time. We recommend an intuitive name that clearly identifies the SNE in the Site Management Portal UI and Metasys site.