Metasys network sites - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

A small Metasys network site comprises a single SNE or multiple SNEs, SNCs, and NAEs with one of the SNEs designated as the Site Director (Figure 1). See Site Director for additional information on Site Director hierarchy and the number of network engines a Site Director can supervise.

Figure 1. Metasys Network with SNE as Site Director for multiple network engines

Larger Metasys network sites can comprise multiple SNEs and one or more ADSs or ADXs with access to multiple remote sites. On any site with one or more ADSs/ADXs, an ADS/ADX is designated as the Site Director. Figure 2 shows an example of a simple Metasys network with one SNE, one NAE55, and an ADS as the Site Director.

Figure 2. Metasys Network with ADS as Site Director for one SNE and one NAE