Metasys Help Files - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

The Metasys Help files provide shared system information and individualized mode-dependent information for the Metasys Site Management Portal (SMP) or the System Configuration Tool (SCT). The Metasys Site Management Portal Help (LIT-1201793) provides information about alarming, commanding, auditing live data values, and other online features. The SCT: System Configuration Tool Help (LIT-12011964) provides information about offline operations such as managing archives, creating spaces, simulating systems, and establishing equipment and serving relationships.

In either SMP or SCT mode, the Metasys Help menu provides Help files in PDF format. Because last minute changes might occur just before product release, always refer to the Johnson Controls Knowledge Exchange for the most up-to-date version of the Metasys Help files.