MS/TP communications bus - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

The MS/TP communications bus is a local or remote network that connects supervisory controllers and equipment controllers to point interfaces using BACnet MS/TP protocol. The remote network, called the Remote Field Bus, requires the addition of a BACnet/IP to BACnet MS/TP Router. The MS/TP bus consists of two types of buses: the FC Bus and the SA Bus. Each bus has its own set of device addresses. For details on how to apply the local and remote MS/TP bus, refer to the MS/TP Communications Bus Technical Bulletin (LIT-12011034) .