Initial default SNE configuration - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

SNEs are configured in the factory with standard initial values for many of the editable attributes. The following table lists some important initial default configuration values for the SNE.

Table 1. SNE Initial Configuration Values

Attribute/Field Name

SNE Initial Value

Computer Name

SNExxxxxxxxxxxx, where xxxxxxxxxxxx is the Ethernet MAC address of the device without hyphens. For example, if the Ethernet MAC address is 00-10-8D-05-0F-FC, the initial Computer Name is SNE00108D050FFC.

DHCP Client

Enabled

Site Director

A new network engine is a Site Director by default. If an SNE is not going to be the Site Director, demote the engine by specifying the Computer Name or IP address of the designated Site Director in this Site Director attribute field.

Initial Login Username

MetasysSysAgent (not case sensitive)

Initial Login Password

Contact your local Johnson Controls representative.