Email notification - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

You can configure an SNE to generate alarm and event messages by sending email to one or more email destinations using the email DDA. The steps require you to configure custom email messages and specify email message destinations in the Email tab of the Site Management Portal UI. The following figure provides an example of an email message destination that is active Monday through Friday from 6:00 A.M. to 6:00 P.M.

Figure 1. Example of defining an Email notification