Controller Configuration Tool (CCT) - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

CCT is a software tool that you use to configure, simulate, and commission equipment controllers that belong to the Metasys system family, such as CGMs, CVMs, FACs, FECs, IOMs, and VMAs. Among the many helpful CCT options is Supervisor Passthru, which provides you the means to download an equipment controller over the Metasys network, provided SCT 15.0 and CCT 15.0 are installed on the same computer. For more information on CCT, refer to the Controller Tool Help (LIT-12011147) .