Editing existing alarm parameters - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document type
Commissioning Guide
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

Procedure

  1. In the Site Management Portal UI, select and drag the required SNE object or field device object from the Navigation panel and drop it in the Display panel. The SNE or field device Focus screen opens.
  2. Click the Alarm tab. The Alarm Configuration screen opens (Figure 1).
    Figure 1. SNE Alarm Configuration Tab
  3. Select items in the Select Item(s) list to edit existing alarms. (To create new alarms, see Creating new alarms.)
  4. Click Edit and make changes to the required Attributes for the SNE or field device.
  5. Click Save to save the edited alarm settings.