Preparing SNE for a network that supports DNS but not DHCP - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

This scenario is not typical of modern networks. The steps are identical to the steps in the Preparing SNE for a network without DHCP and without DNS support when the SNE uses APIPA and Preparing SNE for a network without DHCP and without DNS support when the SNE uses a static IP address.

Using the SNE Ethernet MAC address (from the SNE label), the network administrator can update the DNS server and the assigned computer name. If this is done, you can enter dns-name in Launcher on any computer on the building network.