Preparing SNE for a network that supports DHCP but not DNS - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

About this task

This scenario is common to many building networks. The SNE should only use DHCP without DNS if you have configured DHCP to always assign the same IP address after device resets and lease renewals. If this is not the case, use static IP addresses as described in Preparing SNE for a network without DHCP and without DNS support when the SNE uses a static IP address.

Procedure

  1. Attach the SNE to the network using an Ethernet patch cable.
  2. With your computer or commissioning laptop connected to the building network, open SCT Pro. This tool listens for and shows the IP address information of the SNE as it comes online.
  3. Connect supply power to the SNE and wait for the SNE to complete initialization. SCT Pro indicates the current IP address of the network engine.
    The startup and initialization sequence may take up to 10 minutes to complete.
  4. Go to Installing Launcher to access the SNE, follow all instructions, then return to the next step in this section.
  5. After you have completed the steps in Installing Launcher to access the SNE, including the step for logging in to the SNE, update the SNE computer name value on the Network tab. After the computer name is updated, the Site Management Portal UI automatically logs out, and the SNE automatically resets. Wait for the SNE to complete the startup and initialization sequence. (This sequence may take up to 10 minutes.)