Entering basic SNE parameters in the focus screen - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

Procedure

  1. In the Site Management Portal UI, display the SNE device object and click the Focus tab.
  2. Click Edit. Edit the SNE Object Name and Description values as required.
    Figure 1. SNE Focus tab (Basic)
  3. Click Save.
  4. Select the Advanced option and click Edit.
    Figure 2. SNE Focus Tab - Advanced Edit Mode
  5. Edit the advanced attribute values as needed. (Refer to the Engine Device Object and Audit Trails Help in the Metasys Site Management Portal Help (LIT-1201793) for guidance.)

    If the SNE is on a site with an ADS/ADX, enter the ADS/ADX’s IP address in Local Site Director field in the Site section of this screen. The SNE thereafter reports to the ADS/ADX as its Site Director.

    If you require the USB ports on the SNE for a third-party integration, set the corresponding USB Port to True under the USB Control section of this screen (USB Port 1 Enabled and USB Port 2 Enabled). For details, refer to the Engine commissioning document for your particular integration.