Entering SNE network parameters - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document type
Commissioning Guide
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

The SNE Computer Name and Domain Name on the Network tab identify the SNE on the network so it can be found by other computers. In many commissioning scenarios, you can use the initial Computer Name to commission the SNE. See Computer name for more information.

In most site configuration scenarios, you configure many of the Metasys network values in the SNE UI by downloading a pre-built archive database from the SCT to the commissioned SNE. The download from SCT overwrites the initial Computer Name with the new value for the Metasys network.

Note: If you are building the SNE database online, you must establish the production network SNE Computer Name value before you establish references to objects on the SNE. After creating object references, changing the Computer Name value breaks all object references to local objects on the site.
  1. In the Site Management Portal UI, display the SNE device object, click the Network tab, and then click Edit.
    Figure 1. SNE Network Tab - Edit Mode
  2. In the Network Identification section, type the Computer Name value.
  3. Enter the Network Identification and LAN attribute values as needed and click Save.