Enabling and disabling Warning Banner - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active
Note: If the warning banner for a network engine's Site Director is set to appear, the selected warning banner also appears when users log in to that network engine. Therefore, you only need to follow these steps when the network engine is a Site Director.
  1. In the Site Management Portal UI, display the SNE Site object, click the Site View tab, and then click Edit.
  2. Scroll to the bottom of the window to locate the Warning Banner attribute.
    Figure 1. Enabling and Selecting the Warning Banner - Network Engine Example
  3. Select a banner type from the Warning Banner drop-down box. For a small-capacity engine, only the DoD warning banner is available, so select True for the Warning Banner attribute. For a large-capacity engine, you can select from three different warning banners: U.S. Department of Defense (DoD), U.S. (General Services Administration (GSA)), or U.S. Department of Transportation (DOT) Federal Aviation Administration (FAA). None is selected by default.
  4. Click Save. The banner change takes from 3 to 5 minutes to become effective at the network engine.
Note: If you want to disable the Warning Banner in the future, go back to this screen, select False or None, and save the change.