Enabling Expert mode - Metasys - LIT-12013352 - M4-SNE10500-0 - M4-SNE10501-0 - M4-SNE11000-0 - M4-SNE11001-0 - M4-SNE110L0-0 - M4-SNE110L1-0 - M4-SNE22000-0 - M4-SNE22001-0 - Supervisory Device - SNE10 Network Engine - SNE11 Network Engine - SNE22 Network Engine - SNE Supervisory Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document type
Commissioning Guide
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

About this task

Follow the steps in this section to enable Expert mode in the SMP UI for a Metasys Server or network engine . Expert mode is required if you want to adjust the network sensitivity of the BACnet/IP and MS/TP field bus networks for a network engine (see Adjusting NAE SNE Network sensitivity (LIT-1201519)). The Expert mode options are available to you under the Expert tab of Metasys Preferences. Expert mode is also required to enable web service logging and to view memory usage on the status bar.

Procedure

  1. Start Windows File Explorer and verify that file extensions appear. If file extensions are hidden, click Tools > Folder Options and under the View tab, remove the check box for Hide extensions for known file types.
  2. With Windows File Explorer, navigate to the folder called C:\Users\<user>\JohnsonControls.Metasys, where <user> is the name of the user who is currently logged in to the computer.
  3. Create a new text file called MetasysExpertPreferences.xml under this folder. Make sure that you are saving the file to the C:\Users\<user>\JohnsonControls.Metasys folder. If the file is already present, skip to the next step.
  4. Log on the Metasys SMP. Click Tools > Configure Preferences to open the Metasys Preferences window. The Expert tab is now visible.
  5. Click the Expert tab and set Show Internal items and views to True. Click OK to apply the change and close the window.
  6. Refresh the SMP UI window to allow the Snapshot Focus windows to appear.