Changing Site Director with the SCT - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

Procedure

  1. Start the SCT, open the archive database for the site, and choose the new Site Director from the available list in the Site Director attribute of the Site object.
  2. Perform a download to update all devices. During the download process, pair all Release 10.0 or later network engines with the Site Director. For more information about device pairing in SCT, refer to Metasys SCT Help (LIT-12011964).