Configuring encrypted email with no authentication required - Metasys - LIT-12013352 - M4-SNE10500-0 - M4-SNE10501-0 - M4-SNE11000-0 - M4-SNE11001-0 - M4-SNE110L0-0 - M4-SNE110L1-0 - M4-SNE22000-0 - M4-SNE22001-0 - Supervisory Device - SNE10 Network Engine - SNE11 Network Engine - SNE22 Network Engine - SNE Supervisory Network Engine - 12.0

SNE Commissioning Guide

Brand
Metasys
Product name
SNE10 Network Engine
SNE11 Network Engine
SNE22 Network Engine
SNE Supervisory Network Engine
Document type
Commissioning Guide
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active
Language
English

About this task

Note: Encrypted Email with No Authentication Required functions only when Anonymous Authentication is enabled on the mail server.

Procedure

  1. View a network engine.
  2. Click the Email tab.
  3. Click Edit.
  4. Edit the Attributes in the Shared Configuration as shown in Table 1.
    Table 1. Attributes for No Authentication Required
    Attribute Selection
    SMTP Server Host mail.yourdomain.com or yourdomain.com
    SMTP Port 465
    Authentication Type None
    SSL Email Enabled True
    SSL Email Ignoring Errors False
  5. Verify that the email was sent correctly.