Configuring encrypted email with SMTP authentication - Metasys - LIT-12013352 - M4-SNE10500-0 - M4-SNE10501-0 - M4-SNE11000-0 - M4-SNE11001-0 - M4-SNE110L0-0 - M4-SNE110L1-0 - M4-SNE22000-0 - M4-SNE22001-0 - Supervisory Device - SNE10 Network Engine - SNE11 Network Engine - SNE22 Network Engine - SNE Supervisory Network Engine - 12.0

SNE Commissioning Guide

Brand
Metasys
Product name
SNE10 Network Engine
SNE11 Network Engine
SNE22 Network Engine
SNE Supervisory Network Engine
Document type
Commissioning Guide
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active
Language
English

Procedure

  1. View a network engine.
  2. Click the Email tab.
  3. Click Edit.
  4. Edit the Attributes in the Shared Configuration as shown in Table 1.
    Table 1. Attributes for SMTP Authentication
    Attribute Selection
    SMTP Server Host mail.yourdomain.com or yourdomain.com
    SMTP Port 465
    Authentication Type SMTP
    SSL Email Enabled True
    SSL Email Ignoring Errors False
  5. Verify that the email was sent correctly.