Configuring encrypted email with POP-before-SMTP authentication - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

About this task

Note:

When SSL Email is enabled and you use POP-before-SMTP Authentication, the Metasys system uses port 995 to communicate to the mail server. Ensure that the mail server you are connecting to uses port 995 for secure socket layer connections for POP3 access.

When SSL Email is not enabled and you use POP-before-SMTP Authentication, the Metasys system uses port 110 to communicate to the mail server. Ensure that the mail server you are connecting to uses port 110 for non-encrypted POP3 access.

Procedure

  1. View a network engine or device.
  2. Click the Email tab.
  3. Click Edit.
  4. Edit the Attributes in the Shared Configuration as shown in Table 1.
    Table 1. Attributes for POP-Before-SMTP Authentication
    Attribute Selection
    SMTP Server Host mail.yourdomain.com or yourdomain.com
    SMTP Port 465
    Authentication Type POP-before-SMTP
    POP Server Hostname yourdomain.com or pop.yourdomain.com
    SSL Email Enabled True
    SSL Email Ignoring Errors False
  5. Verify that the email was sent successfully.